EIP.PLLMODE
Description
When the CIP Sync connection is made by the PLC, the EIP.PLLMODE is automatically set to 1 (CIP Sync). The value can be queried in the WorkBench terminal.
This parameter reads the Phase-Locked Loop (PLL) mode.
| Value | Description |
|---|---|
| 0 | Off - Not synchronized |
| 1 | Synchronized with CIP Sync connection |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-10-00-000 |
General Information
|
Type |
|
|
Units |
|
|
Range |
|
|
Default Value |
|
|
Data Type |
|
| See Also | |
|
Stored in Non-Volatile Memory |
|
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Industrial Ethernet
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3900 |
1 |
3900 (0xf3c) |
EIP.PLLMODE |
Unsigned8 |
Read/Write |
Yes |